Other Parts Discussed in Thread: BQSTUDIO
Hi Guys
I have gone through the following excellent topic thoroughly "https://training.ti.com/gauge-programming-fundamentals"
Unfortunately the gauge parameters required for configuring there are slightly different. Nevertheless...
I have attached my battery to the EVM, fired up bqStudio and configured the following (under Data Memory -> Gas Gauging):
(*) - Design - Design Capacity mAh (850 mAh)
(*) - Design - Design Voltage (3700 mV)
- FC - Set Voltage Threshold (4200 mV -> my battery requires this as the CV voltage for charging)
- FC - Clear Voltage Threshold (4100 mV -> following suite of the default parameters)
- State - Qmax Cell 1 (850 mHh -> even though I change design capacity, this still keeps default of 5359 mAh, which would logically appear to be wrong IMHO)
- State - Qmax Pack (same as Cell 1)
(*) - IT Cfg - Term Voltage (2800 mV -> I guess this should maybe be a bit higher than the manufacture specs, as at that point of discharge one starts to damage the battery, but so far no discharge)
Question 1 :
What are the the minimum parameters that need to be changed to make it work for my system? (*) denotes the parameters that I can find that match those mentioned in your guide in the link, but the others I can not find (i.e. 'Taper Voltage' and 'Taper Rate')
Question 2 :
Based on my configuration, bqStudio says that my battery is at 25% SOC. I am assuming that this is because it has already charged my battery to max capacity with the incorrect parameters first, and now that it may have the correct capacity, it has incorrect book-keeping...so how do I restart this? Do I need to discharge the battery?
Question 3 :
The device I am working on will be a compact device, and will house the battery inside (non-removable), with the bq27750 on a PCB connected via I2C to a microcontroller. As such, I dont beleive it will be possible to use the bqStudio 'Golden Image' for pre-production configuration...is my beleif correct? Is it standard practive for devices to program the gauge upon start up first time, with battery connected, if parameters are not right?
Thanks for your time.
Regards,
Eugene