Other Parts Discussed in Thread: BQ27510
Using a Lithium Ion battery and the BQ24075 battery charger, when USB power is supplied, the charging current does not get to the expected level. I have the EN1 and EN2 pins configured for 500mA charging limit, SYSOFF and CE are driven low to enable charging.
When a charger is plugged in, the charge current is ~90mA with 30mA system draw. Following the battery charging flow diagram in the datasheet, the charger gets stuck waiting for I(BAT) < I(TERM) and T(FASTCHARGE) elapses, causing #CHG to flash. The battery is being charged, but at a much slower rate than expected.
I have tested with different batteries at different voltages(3.0V - 4.0V), different boards (using a custom board, schematic below), different USB sources, and different EN1 and EN2 configurations. All yield the same results.
This is being used in conjunction with the BQ27510 fuel gauge, but I have ruled that out.