Hi,
I am trying to power Sony camera through a GP5 relay, the device used inside it is TPS62110, the camera takes 12V and is rated for 1.5W, . Sometimes the Camera do not turn on even after the relay is closed, to turn on the camera command to close relay is send again the relay bounce time is 2ms. Has it to do with UVLO and the bounce time? CAn some one provide some insight into this.?