Hi, I'm using BQ34Z100-G1 with Battery ICR18650-30B spec:
1. Nominal voltage : 3.78V
2. 4-cells
3. cell capacity : 2950mAh
The gas gauge settings are:
1. Design Cap=7080 (60% of battery capacity)
2. CC Threshold=6372 (90% of Design Cap)
3. Design Energy=2620
4. Energy Scale=10
But, it doesn't update the learning status to 5 after fully charged (charging current is about 500mA).
Thank you for your help.