Tool/software: WEBENCH® Design Tools
Dear Support from Texas Instruments,
I have a question referring to Design 4491542/3 UCC28630DR
and I would like to implement the following transformers because I have no clue how to build a transformer myself.
Würth offered me the following Transformers to use 760871135, 750871032, I calculated with the simple transformer equation and given voltages from the webench and with the used ratio provided by würth I get 11,89V Usecundair at a output current of 6.6A.
however I dont know if its correct. can this be validated in Webench or is there another way?
the output voltage is not that critical but should be inbetween 12V till 48V.
sincerely yours
Bastiaan Pierik