Hi All,
I have designed Charging ckt. for lead acid battery of 24V, 7.2A rating, and maximum charging current(Imax-chg) is 2.5A .
The problem is getting current not more than 500mA, headroom for input voltage is also not an issue, Input voltage is 4V more than output voltage. What i expect is battery should charge with current of 2.5A.
I have attached schematic of my designed circuit please go through it, and correct me if i was wrong somewhere, any help will greatly appreciated.
And one more problem is about measuring voltage of STAT1 pin, while mode change. is that voltage range mentioned in datasheet of bq24450??
Hoping reply ASAP!!!
Thanks,
Prashant C