This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: CC gain/capacity gain values

Part Number: BQ78350-R1

Did someone also experience an issue while manually trying to write a CC gain or capacity gain values that are lower than 1mOhm to the BQ78350-R1 component? (The component is supposed to support minimum values down to 0.1 mOhm). I am using the Battery Management Studio version 1.3.52.

Currently writing CC gain or capacity gain values lower than 1 mOhm is only possible by using the calibration option.

Thanks!