Dear All:
I am using the BQ76940 to design the 14S BMS can you answer the following questions?
1. From sleep mode to normal mode, reading the parameters requires a delay of at least 800ms?
2. Does it need to initialize for each wakeup from sleep or only need to initialize for the first time?
3,if the balance is not turned off, will the cell run out ?
4. whether the BQ76940 needs to be protected by temperature during balance?and if yes how to do?