This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24725AEVM-710: Charging battery with EV2400 and BQ24725A GUI

Part Number: BQ24725AEVM-710
Other Parts Discussed in Thread: BQ24725A, EV2400

Hello,

I have the BQ24725A hooked up with the EV2400 and 2 batteries in a 2s1p configuration. I have the DCIN of the EVM at 20V and the Bat load is connected with a multimeter and the battery. The SMBUS off of the EV2400 is connected to the EVM as well with another 3.3V powering that portion of the EVM. I am unable to charge the battery, and writing to the Charge Voltage or Charge Current portions of the GUI do nothing to the system. I read no current at any time. How can I resolve the charging issue?