Hi,
I finished one 8kW PFC design controlled by UCC28070, everything is good except following situation;
1 when DC output power jump from 0 to 8kW, the Mosfet is broken up.
2 when DC output is short circuit, the Mosfet is broken up.
guess: because the DC voltage drops a lot, then the current loop reference is add additional amount to get quick response. but, the peak current limit should work, or because the 90% duty circle with high current make the current transformer saturated?
really need help.