This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33603: Rrt Values - Calculated vs. Table 3 & Table 4 Values

Part Number: LMZM33603

Hi.  I'm wanting to use an external clock sync on the LMZM33603.  From the preliminary datasheet (SNVSAO6) dated 9/2017, I see a table of values for the switching frequency vs. the Rrt value.  However, when I use the formula (3) to calculate the values they do not match the table values.  For example, If I want to switch at 500kHz rather than the default of 400kHz, the formula calculates to (40200/500)k - 0.6k = 79.8kΩ.  But the tables gives a value of 78.9kΩ for this frequency.  the default (400kHz) does work out correctly to a 100kΩ resistor.  I checked a few other frequency values as well and they don't match the formula.  Which values should I use and is the formula correct?