Other Parts Discussed in Thread: UCC25600, , TIDA-01494
There is a new series of LLC resonant controller ICs although the old one, the UCC25600, is still available.
Does the UCC25600 have some advantages over the new series. Which one is recommended for new designs?
Reference designs using the UCC25600 always use an additional gate driver IC (like UCC27714D, up to 4 A drive and sink current). None of the UCC25630X reference designs uses an additional gate drive. This is especially surprizing as the UCC25630X series have less gate drive and sink currents than the UCC25600 (0.6 to 0.8) and far less than an external gate driver.
Has the omission of the gate driver IC something to do with the automatic dead time feature of the UCC25630X?
Is the lack of current and therefore less steep switching slopes compensated by longer dead times?
Would the automatic dead time feature work with an additonal gate driver?
Thank you for your effort.
Paul Hoffmann