This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: Output Layout Design for 28A current output

Part Number: TPS53355

Hi,

I am using TPS53355 to generate 28A, 1V output in one of custom designs. 

Post layout power integrity analysis is failing between regulator output and the inductor, due to high current density and high via current.

For fixing this issue, I would like to understand how to place vias and shapes for that power net.

So please share the board file ( preferably in .brd format) of any of the EVBs which are designed and tested for more than 28A current.

I could find one EVB: TPS53355EVM-743, designed for 30A, but I could not find its board file.

Thanks & Regards,

Madhu