Tool/software: WEBENCH® Design Tools
Hi Team,
my customer wants to use the LM5141 in an application where input voltage is 11-24V and output voltage should be 10.5V. The website states that LM5141 supports 99% duty cycle while I don't find that value inside the datasheet. Webench says the device is limited to 85% and doesn't wont to simulate. Can you please clarify if the device can be used in that application?
Best regards,
Simon