Other Parts Discussed in Thread: BQ4050
Hello,
recently there was a post about the minimum amount of cells that should be connected to this chip. I read that it is recommended, to use more than 2 cells. The BQ76920 is designed to use 5 cells.
In my case Im having a battery, which has 4 cells in series, so I think this should be also okay, I guess?
My question is, what should I do with the input pin which is not connected with a cell? Should I connect it to ground, leave it unconnected or should I do something else with this pin?
Thanks for helping.