This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: BQ76940

Part Number: BQ76940

Good morning,

I'm developing a charger with the BQ76940, for 15 batteries with 4.2V each, totaling a pack with 63V.

However for the design, must use the USB charger type C with 20V 5A.
Is it possible to recharge the battery pack?

  • Hi Andre,
    Be aware the bq76940 is not a charger, it is a monitor device intended to be connected to the cells to monitor voltage, current and temperature. I would expect your charger would include a converter to increase the voltage from the USB type C level to the charging voltage for your battery assembly.