Other Parts Discussed in Thread: BQSTUDIO, BQ34110, BQ34Z100-G1, GPCCEDV
Dear Colleagues,
I have 3S Li-in batteries that I want to use BQ40Z50-561 to charge / monitor. As the battery is packaged with only V+(9-12.7), V-, and 3 SMB lines, how should I connect / configure for the board to work properly with the Battery Management Studio? I connected the battery V+ to 3P, V- to 1N and shorted 3p and 4p, Connected Pack+ / - to a 15V power supply. When all drivers are installed, the Battery Management Studio seem to talk to the board, but I cannot see any charging going on, the power supply keeps showing 0 current, and the voltage between 3P and 1N is 2.7V. Should I add resisters between 1p/1n and 2p/2n?
Many thanks,
Ziwen