Part Number: LP38691-ADJ
Other Parts Discussed in Thread: LP38691,
Hello,
I've see your answer to previous similar question, but I was too busy to answer you..
Neitheless I found differents working of the same component on the same board !!!
On the board we made, the same regulator is use five times, with the same
common input power supply ( Stepdown converter) four of them have no working
current limitation on a shortcut of the output, the 5th will operate correctly !!
I use it on separates prototype board and it also operate correctly...
The only thing that may change is PCB track lenght which are very short to the output ..
they are less than 14mm, the other that have no problem has copper track lenght of
76mm (some with and some without via )...
Another board I made has a total lenght of 55mm with 2 0R resistor and some via
on the power path.....
Does this may help to have a correct working of the component ?
I may send you a partial view of each routing where the LP38691 is used if needed..
thanks for support.
Thierry