Hello folks.
I'm using a TPS61085 boost converter to power some 12 volt fans from a 3.3 volt supply. The fans draw a total of 0.34A at 12 volts. The question I have is how hot should the converter be? With an ambient temperature of 24 degC, its case has reached 64 degC. I have a goal of operating this supply up to 55 degC ambient, and I'm worried that this will be too hot for the converter. I've also measured the inductor and diode temperatures, which are 38 and 32 degC respectively.
The power supply design is nearly identical to that described in figure 12 of the TPS61085 datasheet (here: http://focus.ti.com/lit/ds/slvs859/slvs859.pdf ), although I have substituted to use in-house components where possible.
Is it possible to dissipate some of the heat out of the converter's leads into a copper plane or tracking, and if so which of the leads would be best?
As an aside, I've implemented speed control by using MOSFETs switch in different resistors between the feedback pin and ground. It works quite well, and appears to be an effective way of controlling the fan speed.
Best Regards,
Chris