We are using TPs65930 to power OMAP3503 in our board.
We had built two protos of design and we did not had any issues with TPS65930 power supply. But in our new prototype, we are observing strange behaviour where we see also TPS65930 goes below spec after running for random time ( 30 minutes to few hours).Voltage measurement during running state and failure condition is as below.
|
Working condition |
Not working Condition |
|
|
Voltage on 502 Board |
Measured Value(Volts) |
Measured Value(Volts) |
|
3.3V (Vcc3p3) input to tps |
3.291 |
3.241 |
|
3V (vdd-vmmc1) |
3.158 |
2.959 |
|
1.8V(Vcc1p8) |
1.81 |
1.677 |
|
1.3V (vpll1-1p3) |
1.794 |
1.781 |
|
1.2V(vdd2-core) |
1.207 |
1.191 |
|
1.2 (VOCORE-1P3) |
1.21 |
1.192 |
|
VDD18-USB-PHY(Vaux2) |
1.807 |
1.791 |
Could you please let us know what can be possible reasons to behave like this?