This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5947: Confirm Per Channel Current Limit

Part Number: TLC5947


Greetings -

I'm currently working on an LED display design, and one of the parts I am evaluating is the TLC5947.

What I would like to confirm is, can this part (DAP with exposed pad soldered) handle all 24 channels running 30mA per channel.  More than likely these will only be running 25mA (85% max per channel).  I ask because in the past I have run across TI parts that have total current limits.  So you may have 8 or 16 channels available at 30mA  each, but you can only run 120mA total through the part.  I want to confirm that this part can in fact run 30mA per channel with all 24 channels, so long as you abide by the power dissipation restrictions.

Thanks much!

JB