This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: Does TPS54302 have Load current limit function?

Part Number: TPS54302
Other Parts Discussed in Thread: TPS54320,

Dear Sir, the TPS54302 is a  4.5-V to 28-V input voltage range, 3-A synchronous buck converter. If my load condition is 12V/3.1A, what things will happen? I hope TPS54302 has current limit function. If Load current exceed the 3A or some current value, the TPS54302 can enter protect mode to stop output current. But I do not know whether TPS54302 has current limit function? If TPS54302 has the current limit function, what is the average load current value that will break off the TPS54320? By the way, my load is a 12V DC motor and the output voltage of TPS54302 is 12V . Thanks.