Hello,
Im trying to understand what is going on in the User Guide on page 16. There are several examples, which Show me, when balancing adjacent cells is okay.
My problem is here:
"As an example, assume all cells are at 4V. If cells 4 und 5 are balanced the VC3 input pulls to Vc4, which is approximately the cell 4 voltage or 16 Volt. This is within the singel-ended
Maximum voltge of 3x7,2V=21.6V VC3-VC2 voltage doubles, or is 8V; this is within the 9V absolute Maximum differential voltage for this input pair. "
Question 1: What does this mean: VC3 pulls to VC4?Has the VC3-pin the voltage of (cell 4 and cell 5) together?
So in this example, VC3 would have 8 Volts, if we measure between VC3 and ground, right? But as you can see, it is written that is has 16 Volt. Where does the 16 Volt come from?
The cell 4 voltage is 4 Volts. If we balance cell 4 and cell 5, VC3 cant have the voltage of cell 4 ( cell 5 is missing then
As you can see there is a lot of confusion, I guess.