Hi
Could you check the following understanding is correct?
1. Re-charging is run when battery voltage is below VRCH while input source (adapter or usb) is connected. Is it correct?
2. If the TS monitoring is not used, TS can be connected to VSS with 10Kohm resistor. Is the re-charging like question 1 can be functional even when TS monitoring is disabled?
3. Is there any other condition to be run re-charging?
BestRegards