Other Parts Discussed in Thread: PCM1681
Hello,
We working on a project in which audio takes from USB and split audio in 8 channel to get output on 8 x XLR connectors. In the project PCM1681 takes 4 stereo input from DSP (Via I2S Communication).
Output of PCM1681 (8 x Vout) feed in to 8 x DRV135 to get output on XLR connector.
Also, need to show audio level coming out from PCM1681. For that we are using RGY 3-LED level indicator (Mfg. P/N: 5640200132F) and LM3914 Dot/Bard LED Driver.
Functions of LEDs for each XLR output is:
Volume Low -> Green; Volume Typical -> Yellow; Volume High -> Red
So, please review the circuit and confirm below:
- When the LED will be ON
- will it be solid or
- flickering can be seen
- We need to set three level of Volume. How can we set three level of Volume?
- According to following diagram, are the connection of LEDs OK? Please review the attached schematic
- Voltage rating of LEDs : 1.9V Green, 1.7V Red, 1.8V Yellow
Also, please let us know if there is any other way/ part available that we can display audio level as we have only 3-LEDs.
Thank you.
Best Regards,
Aman Shah