Hi,
I am looking for programmable voltage mode controllers for Active clamp (high side clamped) forward and flyback topologies. By "programmable" the following offline features are meant:
(i) Controller coefficients (eg Kp , Ki , Kd ) for linear controllers,
(ii) Dead time between turning on/off of main and auxiliary switch,
- these features should be configurable off line via appropriate external Resistance/ Capacitance.
For my application: Input voltage range is 24 to 42 V, the switching frequency should atleast be 400 kHz.
Could anyone please suggest a suitable part?
Thank you in advance,
Anindya