This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110EVM-796: Device not acknowledged and in the same time battery discharged by some 30mA in open load.

Part Number: BQ34110EVM-796


Hi, 

I had purchased BQ34110EVM few weeks back, and started testing it. At the first attempt, i was able to detect my device and configure it according to my setup. (FYI: i have a 3S cell configuration of Li ion, communication through EV2300) Things were fine at first, and I was able to discharge my battery through my load at 2.8A too. 

After a small break, when I restarted my setup, I was not able to detect my device anymore! and I also noticed that the BMS was consuming some 30mA from the battery pack, without a load connected across it. I am not able to establish any communication with my device anymore. 

Is my device dead?

how do i check the vitals?

Thanks for the help in advanced.