This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5022-Q1: Webench BOM anomalies ??

Part Number: LM5022-Q1
Other Parts Discussed in Thread: LM5022

Tool/software: WEBENCH® Design Tools

Good day Forum,

I have interesting  in doing a boost design using the LM5022

Using Webench as my refr-design tool  design link here >> https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=6459BBC600BD0D9F

I bought a blank dev board from digikey Part 296-45760-ND

I found anomalies in the Webench Design refr BOM compare to the schematic provided by Webench

Other than attempting to go through all the datasheets to determine the correct values,

 I was hoping that webench is a tool to short-circuit the effort and provide reliable info

Referring to the BOM as per the reference design, here are the variations in component  values -

 Value for-                 Schematic Value            BOM PartNumber (digikey)                BOM Properties

Ccomp2                    56.0nF                            1206A562JA = 5600pF = 5.6nF          56.0nF

Ccs                            1.0nF                              04025A101JA =100pf                           1.0nF

I hope someone from Ti / Webench can respond

Thanks!

Gerhard

  • These are typos, either in the schematic values or in the BOM list part numbers. I am checking with our Webench expert and will get back a confirmation of the correct info for you. Please check back.
  • Hi Gerhard,
    In this specific case, the value for the components recommended is correct but the recommended part number has an issue because of a typo in our database. This issue is specific to AVX parts in the design. We are working on a fix for this and will update our database as quickly as possible. In the meantime, you can go to select alternate part and select a non-AVX capacitor and the part number recommended should be correct.
    Regards,
    Gerold
  • Hi All,

    Thank you for the replies.

    You confirm that -

    1.  The schematic value is correct

    2. Problems with AVX Part#

    I have selected Alt comp, not from AVX.

     The correct Part# now follows what the component value is on the schematic.

    Thank you.

    Gerhard Laubscher

    Cape Town, South Africa