This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206: VREF accuracy of TPS51206

Part Number: TPS51206


Hi,

We got a question from customer about TPS51206.

Could you help us?

Could you tell me the VREF accuracy of TPS51206.

The accuracy of VREF is ± 1.25% in the worst case.

If output current and temperature are limited as follows, can the output voltage error be within ± 1%?

-Temperature range: 0 to 75 ℃

-Output current: within 5 mA or within 3 mA