This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A47: SENSE, OUT pin Absolute maximum ratings

Guru 20090 points
Part Number: TPS7A47


Hello,

Are there any problem if there is 0.7V voltage on the SENSE and the OUT pin when the IN and the Enable pin input is 0V?
Since the SENSE and OUT pin absolute maximum voltage is -0.4V to +36V, I think that there is no problem.
If there is no problem, is there no ESD protection diode between SENSE / OUT and VIN?

Best Regards,
Ryuji