Part Number: TPS54821
Dear all ,
There is something confusing about tps54821 using.The follow decription is found from it's datasheet:
The EN pin has an internal pull-up current source that can be used to adjust the input voltage
under voltage lockout (UVLO) with two external resistors. In addition, the EN pin can be floating for the device to
operate with the internal pull-up current.
1 how many is the internal pull-up current?
2 If the EN pin is controlled with the PG signal of the front stage power supply,can it be directly connected without the pull resistance????ou
Many thanks ! and looking forward to your reply!!!