This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for recommendations for Wireless Charging solution

Other Parts Discussed in Thread: BQ500212A, BQ50002, BQ500511, BQ51051B

Hello,

   I'm at the beginning stages of a product, and I need a wireless charging solution, both Tx and Rx. 

Tx: looking for <5W transmit

Rx: looking to charge a Li-Ion battery, 4.35V, 0.5A charge current.

On the transmitter, the BQ500212A is available, but NRND. There's also the BQ500511/BQ50002 combination, but that's NRND too. Is TI getting out of the wireless power business? If not, what parts should I use?

For the receiver, the BQ51051B looks appealing because it has integrated charging. Will this part be NRND soon? Is there a better solution?

Thanks,

Derek