This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54428: For VIN=5V, Vout=3.3V

Part Number: TPS54428


Hi team,

 

I'm using webench simulation of TPS54428, but it's not avaible to simulate it from IOUT=2.2A (VIN=5V/ Vout=3.3V) in the webench.

So, TPS54428 can't support the following conditions?

 

VIN = 5V

VOUT=2.5V / IOUT = 2.5A (average)

 

Thanks,

Sam Lee