This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150: Start UP sequence of V(VCOM), C(CPI)

Guru 20090 points
Part Number: TPS65150


Hello,

Could you please elt me know the delay time from V(CPI) to V(VCOM)?
In the datasheet P.18 figure 12, there is no delay time.
However in the customer measurement result, there is the 5ms delay from V(CPI) stabled to V(COM) start up.

Best Regards,
Ryuji

  • Hello Ryuji,

    Thanks for your request. Could you prove this with a scope plot? Could you as well provide the schematic (if you do not want to share this you can send it to me via email)?

    Thank you.
    Best Regards.
    Ilona
  • Hello Ilona san,

    I will check the schematics and plot and share with you.
    If you have the typical information for this delay time, I appreciate if you would share the information.

    Best Regards,
    Ryuji
  • Hello Ryuji,

    In Figure 26 on page 30 in the datasheet you can see that there is no delay between V(VGH) and V(VCOM).
    V(CPI) should not be used by the customer, he should use V(VGH) instead. There is a direct connection from V(VS) to V(CPI) through the diodes, so V(CPI) will start at the same time as V(VS), but will only switch when td(DLY2) has passed. Is it possible that your customer is using V(CPI) as output and not V(VGH)?

    Best regards,
    Brigitte
  • Hello Ryuji,

    Is there any update on this issue?

    Best regards,
    Brigitte
  • Hello Brigitte san,

    Sorry. I couldn't get any reply from the customer.
    I will let you know if I got the update from the customer.

    Best Regards,
    Ryuji
  • Hello Ryuji,

    Thank you very much for the information. I will close the thread for now, just post a reply below (or create a new thread if the thread has locked due to time-out) if you hear back from your customer.

    Best regards,
    Brigitte
  • Hello Brigitte san,

    I appreciate your support.
    I will reply or create new thread if I got any information from the customer.

    Best Regards,
    Ryuji