This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R2-DEVICE-FW: Revision Two BQZ File not working for calibration, again..

Part Number: BQ78350-R2-DEVICE-FW
Other Parts Discussed in Thread: BQSTUDIO

It seems that everyone having issues with the calibration procedure got a new BQZ file to make it work under R1. I've upgraded to the R2 firmware and the calibration procedure is broken in the same way. 

Message: "Raw Calibration Block Size Returned after command 0xF081 or 0xF082 is an incorrect length."

Do you have a new BQZ file that will allow calibration for R2 firmware? 

thanks!