Part Number: TPS22933
Hi Folks ,
i have one question regarding the operting temperture of this part .
I want to use this Part at a PCB which will be operated up to 120°C Board Temperature with an Air Tempertur flowing around the PArts with up to 70 °C Ambient.
Is it possible to use this part at my PCB without damagin it ? Because the Datasheet only states the free air temperture operating range of -40 ° C to 85°C , the junction temperture is higher i guess ?
Thank and greetings