Other Parts Discussed in Thread: BQ24075,
Hello,
I have an application where I might want to use the bq24075T to charge a battery at 190 mA. I noticed that the bq24075T datasheet has a specified minimum of 300 mA (R_ISET = 3 kohm), whereas the bq24075 is specified down to 100 mA (R_ISET = 8.9 kohm).
Can you verify that the accuracy of bq24075T is only suitable for R_ISET >= 3 kohm Or can the bq24075T support the same fast charge range and accuracy as bq24075?
The two devices seem very similar, so I was wondering if perhaps the bq2407xT datasheet was never updated, as the new, lower range for non-T came in a 2014 revision.
Thanks,
Jonathan