Hi,
TPS3710 have VDD=12V and the sense input is driven by 3.3V GPIO of uC/FPGA.
I am looking to set up a Raising Threshold Voltage of 2.1V for TPS3710
For this calculations are made with VIT- = 394.5mV and Isense =25nA.
Q1. Please validate the resistor values R1=807.84K and R2=187K can set the Raising Threshold voltage to 2.1V with built-in hysteresis of 5.5mV?
Thanks in Advance
DEEPAK V