Other Parts Discussed in Thread: EV2400
Hello,
Here I have a two questions:
1) When I plug the charger to the board, BQ27621 shows battery level jumped to 30-40% (example: was 19% of battery, after plugging of the charging: 65%). When I unplug the charger, the battery values is starting go down (after minute-two 1% down), but when I restart the board, BQ27621 returns the previous (19%-20% value) - what can be a problem? Is it correct behavior?
2) When I connect the charger to the board, sometimes I get a changing of the flag DSG in the Flags() after about 10-15 seconds - what can be a problem?
Thank you very much!!