This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5026: can't reach to maximum duty cycle

Part Number: LM5026
Other Parts Discussed in Thread: LM5025C

Dear Experts,

I'm working with a LM5026-design. LM5026 is programmed to allow maximum duty cycle, 80%. For some reason LM5026 is not increasing duty cycle beyond ~72%.

DCL is connected to RT.

Voltage in UVLO is 1.3...1.4V.

Free running frequency set by RT-resistor is 250kHz. Design is sync'd externally with 300kHz frequency. Duty cycle of ext sync signal is 50%.

Do you have any ideas what could cause such behavior?

Thanks!

Rgds,

Juha