Other Parts Discussed in Thread: BQ78350
Hello,
refering to the BQ78350 datasheet on page 14, I would like to know what the circuit is about, which is connected to the SMBD and SMBC pin?
I see two spark gaps, two Z-diodes, and to resistors, connected to ground and resistors, which are in series connected between the pin header and the pins of the chip
I could imagine that I need the Z-diodes to stabilize the voltage across SMBD and SMBC.
The sense of the spark gaps is to reduce the ESD to the remaining circuit.
And what are the remaining resistors for? ( 4x 100 Ohms, 4x 1 MOhms)
I could imagine that the voltage at the SMBD and SMBC are measured across this pins and ground. The bigger the resistors R73,R76 the better is the voltage, measured across this pins.
But I have no clue why I need 100 Ohm resistors in this configuration.
Thanks for figuring this out.