TPS709 datasheet shows the summary in the first page: 150mA continuous current, and 200mA peak output current. I do not however find those numbers listed in the Electrical Characteristics table. Should I rely on the summary description rather than table 6.5? Also, if the peak current is 200mA, how can the part limit the current at 320mA typical?
Thank you!