Part Number: LP3918
Dear Support,
I am using the LP3918, and I want to understand few things I could not find in the datasheet.
1. In our application, we intend to use a LP3918 to charge a LiPo battery and power up its internal LDOs. As the battery is being charged, the LDO's get some of that current to power up. I also need to power up a buck/boost converter in my system to produce 5V directly from the battery. What would happen if I am charging the battery, LDO's are ON, and I enable a buck/boost converter directly from the battery node (which is connected to the PMIC)?
2. Say my LIPO battery protection circuit activated and the battery terminals are at 0V. CHG_IN would have say 5V, I press the switch connected as in Figure 3 of the datasheet, what happens?
3. Is there a application note where I connect USB and my device starts charging its battery immediately (the battery can be 0V, or >3V) without MCU intervention to configure the PMIC to the correct LDO voltage, and other configurations? Is there a way to mimic power path control?
Your help will be greatly appreciated.