Hi,
I am using TPS65251 in my application board. Buck1 o/p = 3.8V/2A, Buck2 o/p = 5V/1A, Buck3 o/p = 3.3V/1A, the i/p supply is 12V common to all. Frequency of operation is 500KHz (R on PIN6 = 383K). RLIM1 = 100K, RLIM2 = 120K, RLIM3 = 120K. However, I am not getting the required current limits. Buck1 switches OFF at 900mA, Buck3 switches OFF at 1.4A, I did not check with Buck2. I have tried changing the value of resistance at RLIM1 = 100K/140K/47K/10K, however the current limit on Buck1 remain the same. Same is the case with Buck3. Please help