Hi
Is it possible to set all fault events as latch-off type for TPS2660x family if a 402Kohm resistor is connected between MODE and RTN pins?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Karikalan
Thank you for your reply.
Because I got the following on the datasheet P. 23 9.3.5.3 FAULT Response.
9.3.5.3 FAULT Response
The FLT open-drain output asserts (active low) under following conditions:
• Fault events such as undervoltage, overvoltage, over load, reverse current and thermal shutdown conditions
>On other faults, such as over voltage, under voltage, reverse current etc, it does not latch off.
Is there way to know what fault event is occurred?
BestRegards