This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: Behavior when Vin < Vout

Part Number: LM5116

Dear Team,

my customer would like to know how the device behaves in conditions when Vin < Vout.

Design Parameters:

  • Designed Input Voltage: min. 9V
  • Designed Output Voltage: 7V
  • Input Caps: 4* 4.7 uF
  • Output Caps: 4* 10uF

Now the situation that the input voltage goes down to 6V, so Vin < Vout.

Can we assume how the system will behave?

On the one hand, I assume that the UVLO mechanism will send the device into a Sleep Mode at a certain voltage. On the other hand, the external FETs might have body diodes and the body diode of High-Side FET could be conducting.

Once I had a situation with a High-Side FET system protection where the input voltage was collapsing and with smaller C_in compared to bigger C_outs, the body diode was conducting. 

Any feedback is very much appreciated.

Best Regards
Martin