Other Parts Discussed in Thread: TPS62135
We are using TPS62130 on one of our designs and seeing high leakage when the regulator is not powered up but EN pin is connected to 3.3V externally. My understanding is that the EN pin has intenal pull down of 400K. Is there any other leakage path for the EN pin within the chip? The functional diagram does not show anything else connected to the EN pin. We are assuming there may be a clamping diode between EN pin and input rail which is causing the leakage. We do not have any pull up resistor between Vin and EN pin. Will any other version of EN62130 (drop in replacement) help?