This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24296M: What's the difference between bq24296 and bq24296M?

Part Number: BQ24296M
Other Parts Discussed in Thread: BQ24296

Hi,

What's the difference between bq24296 and bq24296M? I didn't find the difference between them. Please help on this question if you know it. thanks. 

BR,

Eric

  • The differences are:
    bq24296M: Maximum System Regulation voltage is VBAT+80mV; BATFET will not latch OFF for OCP; Default precharge current is 128mA vs. bq24296: Maximum System Regulation voltage is VBAT +150mV; BATFET will latch off for OCP; Default precharge current is 256mA. The REG03 setting is different.