Hello TI,
Since FB internally tracks the TR pin, please could you confirm the working of the PG pin in a tracking scenario? The PG rising threshold is typically 96% - is this of the final FB value (0.7V, when TR >= 0.7V) or is this of the instantanious tracked FB value (TR pin) which could be lower than 0.7V?
Stated differently, is there a possibility of a PowerGood during tracking when TR is less than 0.7V, or can PowerGood only occur once TR reaches 0.7V?
And therefore, once a tracked supply is stable and PG released high, will PG be pulled low if TR subsequently decreases below 0.7V?