Other Parts Discussed in Thread: TIDA-00108, BQ76920, , TIDA-00792
Hello,
I read about the SAFE-Pin, that I can use it to connect an in-line fuse to it. Can you recommend what kind of fuse I could use for this?
If a fault is detected the BQ78350 will switch the state of this Pin to High, is that correct?
Refering to the datasheet of the BQ78350 it is said that: " If the Pin is High, an additional safety protection is given."
With safety protection it is meant, that a fuse can be "activated". Is that right? Or does "safety protection" mean, that it can detect, whether which fault is detected (secondary protection)
If yes how?
Can you show me an example, how to connect the fuse to the Pin and to the battery? Im not sure about this.
I think I need some further informations, to understand this. Unfortunately I havent found a schematic with a fuse.
Thanks for helping me